This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LSF0108:Vref_B 可以#39;t REACH 3.3V?

Guru**** 2943440 points
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/857834/lsf0108-vref_b-can-t-reach-3-3v

器件型号:LSF0108

您好、先生、

下面是我客户的设计和测量

引脚19 = 2.012V
引脚2 = 1.193V

我们能否调整 R196电阻器值以使引脚19变为3.3V?

谢谢