请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TXB0104 你好。
SCES650I 具有以下说明。
第10页
"6.13开关特性:VCCA = 1.8V±0.15V"
最大数据速率 60Mbps VCCB = 5V±0.5V
考虑到60Mbps 为30MHz、
无法通过下图中的40MHz?
此致、
DIE-K
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.