请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN74AVC16T245 大家好、团队:
在 SN74AVC16T245数据表中、上升时间 < 5ns/V;测试条件是什么? 10%~ 90%或20%~80%?
如果客户测量结果为8ns/V、是否可以接受?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、团队:
在 SN74AVC16T245数据表中、上升时间 < 5ns/V;测试条件是什么? 10%~ 90%或20%~80%?
如果客户测量结果为8ns/V、是否可以接受?
谢谢!