This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] SN74AVC2T244:输入端最大绝对电流额定值/Vabs 最大值

Guru**** 2771175 points

Other Parts Discussed in Thread: SN74AVC4T245, SN74AVC2T244, SN74LVC8T245

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/logic-group/logic/f/logic-forum/1298401/sn74avc2t244-abs-max-current-rating-vabs-max-on-input

器件型号:SN74AVC2T244
主题中讨论的其他器件:SN74AVC4T245SN74LVC8T245

我们有一个电路、在目标器件的输入端测量值为 ~-0.84V、重复频率为200kHz、持续时间为~ 5-10ns。

1.对于这种情况对可靠性的影响、我们有什么指导吗?

2.如果电流限制在此输入端低于20mA,这是否会减轻-0.5V 绝对最大负电压限制?

该系列中的类似器件(SN74AVC4T245)在绝对最大值表下方有一条注释(注释2)、指出如果电流受到限制、可能会超过额定电压-该注释是否也适用于此器件? 由于某种原因、它未包含在244数据表中。 请澄清该陈述是否也适用...

从 SN74AVC4T245数据表中:

来自 SN74AVC2T244数据表

谢谢!

史蒂夫