请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SN74AC32 工具与软件:
您好!
最新的 SN74AC32数据表指定了 在4.5V 和5.5V 电源轨下的最小高电平输入电压分别为1.15V 和1.85V。 这两种规格不应该与之前的数据表修订版一样为3.15V 和3.85V 吗?
谢谢!
Naiden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.