请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8300 DRV8300是否可以在1xPWM上工作?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,Nimesh,
由于电源电压高达60V,我建议使用DRV835x设备。 DRV835x系列支持1xPWM模式。 如果您正在寻找类似于DRV8320H的设备,我建议您使用DRV8350H设备。 与DRV8320H相比,DRV8350H器件具有相似的功能集,但我要指出的DRV8350H器件的一个重要区别是它可以支持高达100V的电压,最大ABS为102V。
此致,
Anthony Lodi