请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:DRV8307我想驱动转速为20.000 (12伏,最大60安)的BLDC电机。 我想同时使用DRV8307和MSP430或C2000微处理器。 我想问一下此配置是否可靠,是否可以针对此规格提供任何类型的参考或建议。
此致。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.