请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV2605 主题中讨论的其他部件: DRV2625
我看到的大多数EMR电动机都是3V及以下的电动机,但是像Adafruit和SparkFun这样的I2C板都是5V运行的。 这是故意的,还是不匹配?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.