请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV591 大家好,
我的客户华为使用DRV591驱动TEC,当温度为-40C时,输出电流将达到3A。 他们想知道:
1.在我们的数据表中,最大输出电流为3A (典型值),最小值和最大值是多少? 考虑到老化和可靠性,客户需要预留多少利润?
2.华为的申请是否有问题? 如果输出电流高于3A,对我们的零件有什么影响?
此致,
南方
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.