请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8701 您好,
我很好奇用这个芯片来运行一个90V直流电动机,尽管它的最大电压是47V。 我是否能够将芯片的接地电压设置为大约70-80VDC并运行电机(假设VM为@ 110VDC)? 我假设如果我这样做,Rsense (和其他功能)将不能正常工作,这是正确的假设吗?
谢谢!
垫
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.