请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:ISO5851 我正在尝试将ISO5851栅极驱动器与IGBT (4500V/1200A)1200)栅极驱动器的图腾柱电压源配合使用。
数据表并未告诉我们使用IC的任何限制。 额定电压,额定电流等
我不知道是否可以将IC用于4500V/1200A IGBT1200 IGBT栅极驱动器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.