请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8302 您好,支持团队
客户询问增益设置为40V/v时分流放大器上的体重是多少
谢谢
Jeff Coletti
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好的,Jeff,
让我们来看看这里:
您是指DRV8302的内部电流分流还是EVM的外部分流?
如果它是EVM,它是该电路板吗?
好的,Jeff,
我们发现,SR = 10 V/us时,我们可以大约为10MHz。
此外,如果我们查看数据表的第14页,我们可以计算电流并联放大器的输出,并注意反馈路径中没有电容器。