请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8432 在典型的H桥中,可通过打开高2侧MOSFET并关闭2个低侧MOSFET来实施制动器(反之亦然)。 从数据表中,如果RESET_AB和RESET_CD处于低电平,则所有MOSFET都将处于高Z阻抗。 如何通过DRV8432制动电机?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在典型的H桥中,可通过打开高2侧MOSFET并关闭2个低侧MOSFET来实施制动器(反之亦然)。 从数据表中,如果RESET_AB和RESET_CD处于低电平,则所有MOSFET都将处于高Z阻抗。 如何通过DRV8432制动电机?
谢谢你。