请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8701 尊敬的各位
数据表中允许的SO引脚电容为1nF。 如果将2.2uF置于SO销上,DRV8701是否有任何副作用?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.