请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8662 您好,
我曾使用DRV8662生成200VPP来控制压电负载。
在无负载条件下,当我启用IC时,它给出的输出电压为102V,这是计算得出的vboost值
但几分钟后,vboost值同时下降,IC在无负载的情况下消耗约300mA的更多电流
此外,IC会变得更热,请向我建议一个解决方案。
为供您参考,我附上了设计文件
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.