请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:DRV8871大家好,
您能帮您推荐一些设备给驾驶员螺线管吗?
双通道高侧驱动器,带电流反馈,高达1.5A输出电流,控制频率为3kHz。
如果满足以下要求,H桥驱动器也可接受。
东宝
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.