请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8308 主题中讨论的其他部件: DRV8307
您好,
DRV8308和DRV8307数据表未为CLK50和TBLANK规格指定任何容差;仅指定典型值。 我假定TBLANK时间基于CLK50内置式上升器,因此我可以根据CLK50公差确定TBLANK公差。
是否有任何关于CLK50或TBLANK公差或范围的信息?
谢谢!
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.