请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8412 主题中讨论的其他部件: DRV8432, DRV8840, DRV8711
您好,
我们的客户正在搜索能够输出电流超过3A的步进电机驱动器。
我认为只有DRV8412和DRV8432。
DRV8412是否具有PWM电流控制功能?
客户使用半步进和1/4步进模式。
此致,
Naoki Aoyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.