请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8871 你(们)好
我已经测试过电动机驱动器(DRV8871)。
连接12伏直流电机时工作正常。
但当我更换了24V电动机(VM:24V)时,它不工作。
请告诉我检查点。
它在为不带DRV8871的电动机提供24V直流电源时工作。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.