请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8323 在DRV8323RH驱动器中,是否可以通过设置引脚VREF上的电压来设置电流放大器偏移? 所有电路都显示VREF具有VCC,因此通过将VREF设置为2V是否可以在1伏电压下实现电流偏移?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.