请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV1.0987万 您好,
我使用零件DRV1.0987万作为回转盘电机的驱动器。我从WEBENCH工具得到,在SW引脚中,我需要插入一个47uH的电感器。 板上空间太小,需要最小的电感器。
您推荐哪种电感器?
最大直流电流:1 A
drv1.0987万电压输出为30V。
谢谢!
Liraz Abramovsky。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我使用零件DRV1.0987万作为回转盘电机的驱动器。我从WEBENCH工具得到,在SW引脚中,我需要插入一个47uH的电感器。 板上空间太小,需要最小的电感器。
您推荐哪种电感器?