请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8871 我使用DRV8871驱动刷式直流电机,该电机应在额定电流300mA和失速电流1200mA的7V下工作。
当我测试DRV8871时,它在7V停机时提供的电流不超过500mA。当我尝试增加电压时,驱动器提供的输出电流也增加了,但数据表中提到驱动器从6.5 工作。
请帮助我了解为什么会发生这种情况。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.