请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8320 数据表(使用部件号DRV8320SRTVR)仅指定VM = 6V,8V,10V,13V的高侧VGS和VM = 6V,8V,10V,12V的低侧VGS。 IC设计用于为12V至60V之间的VM值提供什么VGS电压?
谢谢!
尼克
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
数据表(使用部件号DRV8320SRTVR)仅指定VM = 6V,8V,10V,13V的高侧VGS和VM = 6V,8V,10V,12V的低侧VGS。 IC设计用于为12V至60V之间的VM值提供什么VGS电压?
谢谢!
尼克