请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8332 我是否可以提供DRV8332的外部3.3V至VREG引脚,而不 是在DRV8332的VDD引脚上提供12V以降低功耗? 因为VDD用于为DRV8332内部的LDO供电,而DRV8332内部的LDO会产生3.3V电压,从而为DRV8332的内部逻辑电路供电。 此内部LDO的输入为12V,输出为3.3V,因此效率为27.5 % ,效率较差。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.