请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV1.0987万 大家好,
请检查我基于DRV1.0987万的设计,最大输出电流为来自DRV的0.65A,输入电压为30V。
关于电感器,我必须将47uH? 我需要它的体积小 (0603封装),在小footprint.e2e.ti.com/.../DRV1.0987万.docx中很难找到47uH
谢谢!
Shlomi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,
请检查我基于DRV1.0987万的设计,最大输出电流为来自DRV的0.65A,输入电压为30V。
关于电感器,我必须将47uH? 我需要它的体积小 (0603封装),在小footprint.e2e.ti.com/.../DRV1.0987万.docx中很难找到47uH
谢谢!
Shlomi