请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8886AT 主题中讨论的其他部件:DRV8886
大家好,团队
对于DRV8886,要获得最大电流,例如 IFS=2.5A,RREF将为12Kohm,超出规格上的测试条件范围。
客户想确认IFS设置是否仍将遵循方程式1 (7.3 .4)和方程式2 (7.3 .5)。
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.