请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8323 您好,
DRV8323/DRV8321R设备8321设备可以通过SPI寄存器或CAL引脚执行自动偏移校准。
我想通过SPI寄存器使用校准。 PIN CAL的哪种状态? 未连接,连接至GND,连接至3.3V?
谢谢!
Mikaël
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.