请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8711 您好:
请帮助确认以下问题:
1.在正常操作中,步进电机运行到位置时,停止MCU的PWM输出,8711能否锁定电机?电机轴能否旋转。
2.工作状态是否无法关闭24V电源?
3. SPI写入8711的指令是否有详细描述?工作流程是否有简单的解释?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.