请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV595 我现在使用DRV595提供DC输出以驱动DC风扇。 我有一个直流输入电压作为参考。 因为我看到它是差分输入,所以我的潜能值为0伏。 但是,我在数据表中的某些地方看到它必须具有3V偏压,那么当我将接地线接至GND时,我的电路是否工作? 如果是错误的,我希望挽救这一原型。 我的电路也有3.3V电源。 是否可以将电压与3.3V (而不是3V)结合?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.