请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8320 主题中讨论的其他部件:DRV832X
大家好,团队
根据DRV832x的规格,飞线电容器的建议值为47nF。 如果客户使用22nF,该怎么办? 是否存在潜在问题/风险?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.