请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:DRV8908-Q1 尊敬的专家:
客户需要通过"负载转储"测试。 在VM引脚处为64V 50us。
如果他们选择TPSMD28A TVS,OVP将被触发,因为其直流击穿电压最大为34.4V (OVP为33V)
如果他们选择了直流击穿电压为31.9V的TPSMD26A电视,则会在测试过程中灼伤。
他们想知道TI对DRV8908此类测试的建议。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
尊敬的专家:
客户需要通过"负载转储"测试。 在VM引脚处为64V 50us。
如果他们选择TPSMD28A TVS,OVP将被触发,因为其直流击穿电压最大为34.4V (OVP为33V)
如果他们选择了直流击穿电压为31.9V的TPSMD26A电视,则会在测试过程中灼伤。
他们想知道TI对DRV8908此类测试的建议。
谢谢