This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8803:当在 PLC 中用作常规开关时、DRV8803是否支持200kHz 开关速率?

Guru**** 2484615 points
Other Parts Discussed in Thread: DRV8803

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1173045/drv8803-can-drv8803-support-200khz-switching-rates-when-used-as-general-do-in-plc

器件型号:DRV8803

我只会发现"在0kHz 至100kHz 的频率下、可通过脉宽调制来控制电机速度。" DRV8803的数据表中。

我想在设计中将 DRV8803用作低侧开关、开关速率需要为200kHz。

DRV8803能否支持该功能? 或者是否 有任何其他推荐的 IC?