This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8908-Q1:如何配置为4 HS?

Guru**** 2482225 points
Other Parts Discussed in Thread: DRV8908-Q1

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1179197/drv8908-q1-how-to-config-as-4-hs

器件型号:DRV8908-Q1

您好~

客户希望将 DRV8908-Q1用作系统(如 LED、摄像头)的 HS。

它们需要3个0.3A 输出、1个3A 输出。

如果可以、请告诉我吗? 配置它的好方法是什么?

谢谢!

B&R