请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8818 您好!
在评估板设计中、原理图显示了感测引脚处感测电阻两端的100nF 电容。
但 DRV8818的数据表没有提供。
您能否解释为什么添加了它、/在哪些情况下它可能是有益的?
此致、
Fabian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.