请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8353R 主题中讨论的其他器件:DRV8353
大家好、
根据 DRV8353的数据表、MODE/GAIN/IDRIVE/VDS 引脚定义是连接至 DVDD (5V)的上拉电压、
但用户指南建议连接到3.3V。 哪种连接是正确的?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.