请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:MCT8316Z 我们正在使用 MCT8316Z、并希望限制电机的输出电流。
我们将 ILIM 输入设置为1.25V (AVDD/2-0.4)
且 CSA 增益为1.2V/A
在我的理解下、这应该会将电机电流限制为1A。(根据第8.3.12节)
我将示波器放在其中一个电机相位上、甚至可以在相位上看到6安培(PWM 为50-60%)
(更不用说我们烧毁了4个电机)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.