请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8262 我无法为 DRV 8262和 DRV 8962找到具有更高电流容量的 DDV 封装。 它们是否已停产?
另外、该器件更适合在65V、最大电流为20A 的条件下驱动单个有刷直流电机。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.