This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] DRV8353R:故障问题始终会损坏、无输出

Guru**** 2468460 points
Other Parts Discussed in Thread: DRV8353R

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1280144/drv8353r-problem-faults-always-damage-no-output

器件型号:DRV8353R

您好,

我有一位客户使用 DRV8353RS、始终会损坏而没有输出、请帮助了解原因和建议、或更好的器件推荐:

1.设置驱动电流550mA / 1200mA。     

MOS 管型号:FDBL0200N100、Qgd=20nc 。

3、故障症状1: MOSFET 栅极不增加限流电阻 rgen、驱动芯片的驱动电流根据计算(550mA / 1200mA)进行设置、电机运行约2秒钟、驱动芯片无输出(损坏);

故障现象2:MOS 管的栅极加入了10欧姆的限流电阻、驱动芯片的驱动电流按照550mA 管(MOS 1200mA)的计算公式来设置、电机正常运行;

将驱动器芯片的驱动电流调节到最大值(1000mA / 2000mA)、电机运行大约1秒、驱动器芯片无输出(损坏)。

4. 驱动器芯片的详细设置如下所示:

          

     

非常感谢~