低速启动电机时,电机会先提速到更高速,然后再降到目标速度,高速启动电机时,电机会逐渐提速到目标速度,不会超过
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的配置如下:
0x20:0x5C
0x21:0x1A
0x22:0x06
0x23:0x0C
0x24:0x50
0x25:0xC0
0x26:0xB7
0x27:0x00
0x28:0x02
0x29:0x68
0x2A:0x23
0x2B:0x0E
以上配置内容每次上电时都会写入一次,用来保证参数正常。
我使用示波器获取的FG引脚上的输出频率,使用20 μ 启动电机时FG的输出频率会达到90HZ以上,然后降低到64Hz,会在64Hz左右波动,但比较稳定。μ A
但是使用40 μ 启动电机时FG的输出频率会逐渐提高到130Hz,并稳定在130Hz左右,并不会超过这个频率太多。μ A
我的配置:
0x20:0x5C
0x21:0x1A
0x22:0x06
0x23:0x0C
0x24:0x50
0x25:0xC0
0x26:0x87
0x27:0x00
0x28:0x02
0x29:0x68
0x2A:0x23
0x2B:0x0E
电机带负载的条件下,使用IIC发送指定的速度,电机能转得动且速度也可调。但是使用PWM控制速度时,即使PWM输入的占空比达到95 %,电机转速也很低,低于80 %电机启动不了,带不动负载了。