This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] 电机驱动器建议

Guru**** 2463330 points


请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1306680/motor-driver-recommendation

大家好、

我们是否有设备可以满足以下要求?

驱动器电压:3V~5.5V

逻辑电压:2.5V~3.6V

IOT/ch:300mA最小值

应用: x2步进电机

微步进:64 128 256ustep

接口:SPI