请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:DRV8350 大家好、
DRV8350数据表指定了介于 CPL 和 CPH 之间的47nF、VDRAIN 额定值。
可以使用100nF 吗? 这里允许的电容值的范围是多少?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.