This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] LP-MSP430FR2476:TCAN4550演示项目

Guru**** 2988540 points

Other Parts Discussed in Thread: LP-MSP430FR2476, TCAN4550

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/microcontrollers/msp-low-power-microcontrollers-group/msp430/f/msp-low-power-microcontroller-forum/1074240/lp-msp430fr2476-tcan4550-demo-project

部件号:LP-MSP430FR2476
“线程: TCAN4550”中讨论的其它部件

我正在尝试将 TCAN4550项目用于 LP-MSP430FR2476引脚。 我不确定 SPI 设置是否正确。 我没有看到 SPI CS 在范围上激活。 欣赏指针。 SPI 的时钟源为16 MHz。

#include <msp430.h> 
#include "globals.h"
#include "clock~.h"



#define SPI_MOSI_PORT       GPIO_PORT_P3
#define SPI_MOSI_PIN        GPIO_PIN2
#define SPI_MISO_PORT       GPIO_PORT_P3
#define SPI_MISO_PIN        GPIO_PIN6
#define SPI_CLK_PORT        GPIO_PORT_P3
#define SPI_CLK_PIN         GPIO_PIN5
#define SPI_CS_PORT         GPIO_PORT_P2
#define SPI_CS_PIN          GPIO_PIN7
#define SPI_SELECT_FUNCTION GPIO_PRIMARY_MODULE_FUNCTION

volatile uint8_t TCAN_Int_Cnt = 0;                  // A variable used to keep track of interrupts the MCAN Interrupt pin


void init_spi_peripheral(){
    GPIO_setAsPeripheralModuleFunctionOutputPin(SPI_MOSI_PORT, SPI_MOSI_PIN, SPI_SELECT_FUNCTION);
    GPIO_setAsPeripheralModuleFunctionInputPin(SPI_MISO_PORT, SPI_MISO_PIN, SPI_SELECT_FUNCTION);
    GPIO_setAsPeripheralModuleFunctionOutputPin(SPI_CLK_PORT, SPI_CLK_PIN, SPI_SELECT_FUNCTION);
    GPIO_setAsPeripheralModuleFunctionOutputPin(SPI_CS_PORT, SPI_CS_PIN, SPI_SELECT_FUNCTION);




    //Initialize Master
    EUSCI_B_SPI_initMasterParam param = {0};
    param.selectClockSource = EUSCI_B_SPI_CLOCKSOURCE_SMCLK;
    param.clockSourceFrequency = CS_getSMCLK();
    param.desiredSpiClock = 2000000;
    param.msbFirst=EUSCI_B_SPI_MSB_FIRST;
    param.clockPhase=EUSCI_B_SPI_PHASE_DATA_CAPTURED_ONFIRST_CHANGED_ON_NEXT;
    param.clockPolarity=EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_LOW;
    param.spiMode=EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH;


    EUSCI_B_SPI_initMaster(EUSCI_B1_BASE, &param);
    EUSCI_B_SPI_select4PinFunctionality(EUSCI_B1_BASE,0x00);

    EUSCI_B_SPI_enable(EUSCI_B1_BASE);
}

/**
 *  Initialize system clocks
 */
static void init_clock(void) {
    // Configure one FRAM waitstate as required by the device datasheet for MCLK
    // operation beyond 8MHz _before_ configuring the clock system.
    FRAMCtl_configureWaitStateControl(FRAMCTL_ACCESS_TIME_CYCLES_1);

    //Set DCO FLL reference = REFO
    CS_initClockSignal(CS_FLLREF, CS_REFOCLK_SELECT,   CS_CLOCK_DIVIDER_1);
    //Set ACLK = REFO
    CS_initClockSignal(CS_ACLK,   CS_REFOCLK_SELECT,   CS_CLOCK_DIVIDER_1);

    CS_initFLLParam param = {0};
    //Set Ratio/Desired MCLK Frequency, initialize DCO, save trim values
    CS_initFLLCalculateTrim(CS_MCLK_DESIRED_FREQUENCY_IN_KHZ, CS_MCLK_FLLREF_RATIO, &param);

    //Set MCLK = REFO
    CS_initClockSignal(CS_MCLK,   CS_REFOCLK_SELECT,   CS_CLOCK_DIVIDER_1);
    //Set SMCLK = DCO
    CS_initClockSignal(CS_SMCLK,  CS_DCOCLKDIV_SELECT, CS_CLOCK_DIVIDER_1);

    //Clear all OSC fault flag
    CS_clearAllOscFlagsWithTimeout(1000);
}

/*
 * Configure the TCAN4550
 */
void
init_can(void)
{
    TCAN4x5x_Device_ClearSPIERR();                              // Clear any SPI ERR flags that might be set as a result of our pin mux changing during MCU startup

    /* Step one attempt to clear all interrupts */
    TCAN4x5x_Device_Interrupt_Enable dev_ie = {0};              // Initialize to 0 to all bits are set to 0.
    TCAN4x5x_Device_ConfigureInterruptEnable(&dev_ie);          // Disable all non-MCAN related interrupts for simplicity

    TCAN4x5x_Device_Interrupts dev_ir = {0};                    // Setup a new MCAN IR object for easy interrupt checking
    TCAN4x5x_Device_ReadInterrupts(&dev_ir);                    // Request that the struct be updated with current DEVICE (not MCAN) interrupt values

    if (dev_ir.PWRON)                                           // If the Power On interrupt flag is set
        TCAN4x5x_Device_ClearInterrupts(&dev_ir);               // Clear it because if it's not cleared within ~4 minutes, it goes to sleep

    /* Configure the CAN bus speeds */
    TCAN4x5x_MCAN_Nominal_Timing_Simple TCANNomTiming = {0};    // 500k arbitration with a 40 MHz crystal ((40E6 / 2) / (32 + 8) = 500E3)
    TCANNomTiming.NominalBitRatePrescaler = 2;
    TCANNomTiming.NominalTqBeforeSamplePoint = 32;
    TCANNomTiming.NominalTqAfterSamplePoint = 8;

    TCAN4x5x_MCAN_Data_Timing_Simple TCANDataTiming = {0};      // 2 Mbps CAN FD with a 40 MHz crystal (40E6 / (15 + 5) = 2E6)
    TCANDataTiming.DataBitRatePrescaler = 1;
    TCANDataTiming.DataTqBeforeSamplePoint = 15;
    TCANDataTiming.DataTqAfterSamplePoint = 5;

    /* Configure the MCAN core settings */
    TCAN4x5x_MCAN_CCCR_Config cccrConfig = {0};                 // Remember to initialize to 0, or you'll get random garbage!
    cccrConfig.FDOE = 1;                                        // CAN FD mode enable
    cccrConfig.BRSE = 1;                                        // CAN FD Bit rate switch enable

    /* Configure the default CAN packet filtering settings */
    TCAN4x5x_MCAN_Global_Filter_Configuration gfc = {0};
    gfc.RRFE = 1;                                               // Reject remote frames (TCAN4x5x doesn't support this)
    gfc.RRFS = 1;                                               // Reject remote frames (TCAN4x5x doesn't support this)
    gfc.ANFE = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0;                // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for extended ID messages (29 bit IDs)
    gfc.ANFS = TCAN4x5x_GFC_ACCEPT_INTO_RXFIFO0;                // Default behavior if incoming message doesn't match a filter is to accept into RXFIO0 for standard ID messages (11 bit IDs)

    /* ************************************************************************
     * In the next configuration block, we will set the MCAN core up to have:
     *   - 1 SID filter element
     *   - 1 XID Filter element
     *   - 5 RX FIFO 0 elements
     *   - RX FIFO 0 supports data payloads up to 64 bytes
     *   - RX FIFO 1 and RX Buffer will not have any elements, but we still set their data payload sizes, even though it's not required
     *   - No TX Event FIFOs
     *   - 2 Transmit buffers supporting up to 64 bytes of data payload
     */
    TCAN4x5x_MRAM_Config MRAMConfiguration = {0};
    MRAMConfiguration.SIDNumElements = 1;                       // Standard ID number of elements, you MUST have a filter written to MRAM for each element defined
    MRAMConfiguration.XIDNumElements = 1;                       // Extended ID number of elements, you MUST have a filter written to MRAM for each element defined
    MRAMConfiguration.Rx0NumElements = 5;                       // RX0 Number of elements
    MRAMConfiguration.Rx0ElementSize = MRAM_64_Byte_Data;       // RX0 data payload size
    MRAMConfiguration.Rx1NumElements = 0;                       // RX1 number of elements
    MRAMConfiguration.Rx1ElementSize = MRAM_64_Byte_Data;       // RX1 data payload size
    MRAMConfiguration.RxBufNumElements = 0;                     // RX buffer number of elements
    MRAMConfiguration.RxBufElementSize = MRAM_64_Byte_Data;     // RX buffer data payload size
    MRAMConfiguration.TxEventFIFONumElements = 0;               // TX Event FIFO number of elements
    MRAMConfiguration.TxBufferNumElements = 2;                  // TX buffer number of elements
    MRAMConfiguration.TxBufferElementSize = MRAM_64_Byte_Data;  // TX buffer data payload size


    /* Configure the MCAN core with the settings above, the changes in this block are write protected registers,      *
     * so it makes the most sense to do them all at once, so we only unlock and lock once                             */

    TCAN4x5x_MCAN_EnableProtectedRegisters();                   // Start by making protected registers accessible
    TCAN4x5x_MCAN_ConfigureCCCRRegister(&cccrConfig);           // Enable FD mode and Bit rate switching
    TCAN4x5x_MCAN_ConfigureGlobalFilter(&gfc);                  // Configure the global filter configuration (Default CAN message behavior)
    TCAN4x5x_MCAN_ConfigureNominalTiming_Simple(&TCANNomTiming);// Setup nominal/arbitration bit timing
    TCAN4x5x_MCAN_ConfigureDataTiming_Simple(&TCANDataTiming);  // Setup CAN FD timing
    TCAN4x5x_MRAM_Clear();                                      // Clear all of MRAM (Writes 0's to all of it)
    TCAN4x5x_MRAM_Configure(&MRAMConfiguration);                // Set up the applicable registers related to MRAM configuration
    TCAN4x5x_MCAN_DisableProtectedRegisters();                  // Disable protected write and take device out of INIT mode


    /* Set the interrupts we want to enable for MCAN */
    TCAN4x5x_MCAN_Interrupt_Enable mcan_ie = {0};               // Remember to initialize to 0, or you'll get random garbage!
    mcan_ie.RF0NE = 1;                                          // RX FIFO 0 new message interrupt enable

    TCAN4x5x_MCAN_ConfigureInterruptEnable(&mcan_ie);           // Enable the appropriate registers


    /* Setup filters, this filter will mark any message with ID 0x055 as a priority message */
    TCAN4x5x_MCAN_SID_Filter SID_ID = {0};
    SID_ID.SFT = TCAN4x5x_SID_SFT_CLASSIC;                      // SFT: Standard filter type. Configured as a classic filter
    SID_ID.SFEC = TCAN4x5x_SID_SFEC_PRIORITYSTORERX0;           // Standard filter element configuration, store it in RX fifo 0 as a priority message
    SID_ID.SFID1 = 0x055;                                       // SFID1 (Classic mode Filter)
    SID_ID.SFID2 = 0x7FF;                                       // SFID2 (Classic mode Mask)
    TCAN4x5x_MCAN_WriteSIDFilter(0, &SID_ID);                   // Write to the MRAM


    /* Store ID 0x12345678 as a priority message */
    TCAN4x5x_MCAN_XID_Filter XID_ID = {0};
    XID_ID.EFT = TCAN4x5x_XID_EFT_CLASSIC;                      // EFT
    XID_ID.EFEC = TCAN4x5x_XID_EFEC_PRIORITYSTORERX0;           // EFEC
    XID_ID.EFID1 = 0x12345678;                                  // EFID1 (Classic mode filter)
    XID_ID.EFID2 = 0x1FFFFFFF;                                  // EFID2 (Classic mode mask)
    TCAN4x5x_MCAN_WriteXIDFilter(0, &XID_ID);                   // Write to the MRAM

    /* Configure the TCAN4550 Non-CAN-related functions */
    TCAN4x5x_DEV_CONFIG devConfig = {0};                        // Remember to initialize to 0, or you'll get random garbage!
    devConfig.SWE_DIS = 0;                                      // Keep Sleep Wake Error Enabled (it's a disable bit, not an enable)
    devConfig.DEVICE_RESET = 0;                                 // Not requesting a software reset
    devConfig.WD_EN = 0;                                        // Watchdog disabled
    devConfig.nWKRQ_CONFIG = 0;                                 // Mirror INH function (default)
    devConfig.INH_DIS = 0;                                      // INH enabled (default)
    devConfig.GPIO1_GPO_CONFIG = TCAN4x5x_DEV_CONFIG_GPO1_MCAN_INT1;    // MCAN nINT 1 (default)
    devConfig.FAIL_SAFE_EN = 0;                                 // Failsafe disabled (default)
    devConfig.GPIO1_CONFIG = TCAN4x5x_DEV_CONFIG_GPIO1_CONFIG_GPO;      // GPIO set as GPO (Default)
    devConfig.WD_ACTION = TCAN4x5x_DEV_CONFIG_WDT_ACTION_nINT;  // Watchdog set an interrupt (default)
    devConfig.WD_BIT_RESET = 0;                                 // Don't reset the watchdog
    devConfig.nWKRQ_VOLTAGE = 0;                                // Set nWKRQ to internal voltage rail (default)
    devConfig.GPO2_CONFIG = TCAN4x5x_DEV_CONFIG_GPO2_NO_ACTION; // GPO2 has no behavior (default)
    devConfig.CLK_REF = 1;                                      // Input crystal is a 40 MHz crystal (default)
    devConfig.WAKE_CONFIG = TCAN4x5x_DEV_CONFIG_WAKE_BOTH_EDGES;// Wake pin can be triggered by either edge (default)
    TCAN4x5x_Device_Configure(&devConfig);                      // Configure the device with the above configuration

    TCAN4x5x_Device_SetMode(TCAN4x5x_DEVICE_MODE_NORMAL);       // Set to normal mode, since configuration is done. This line turns on the transceiver

    TCAN4x5x_MCAN_ClearInterruptsAll();                         // Resets all MCAN interrupts (does NOT include any SPIERR interrupts)
}


/*
 * GPIO Initialization
 */
void
init_gpio()
{

    GPIO_setAsOutputPin(   GPIO_PORT_P1, GPIO_PIN_ALL8);
    GPIO_setAsOutputPin(   GPIO_PORT_P2, GPIO_PIN_ALL8);
    GPIO_setAsOutputPin(   GPIO_PORT_P3, GPIO_PIN_ALL8);
    GPIO_setAsOutputPin(   GPIO_PORT_P4, GPIO_PIN_ALL8);
    GPIO_setAsOutputPin(   GPIO_PORT_P5, GPIO_PIN_ALL8);
    GPIO_setAsOutputPin(   GPIO_PORT_P6, GPIO_PIN0 | GPIO_PIN1 | GPIO_PIN2);

    // Set all GPIO pins to output low to prevent floating input and reduce power consumption
    GPIO_setOutputLowOnPin(GPIO_PORT_P1, GPIO_PIN_ALL8);

    GPIO_setOutputHighOnPin(GPIO_PORT_P2, GPIO_PIN_ALL8);

    GPIO_setOutputLowOnPin(GPIO_PORT_P3, GPIO_PIN_ALL8);
    GPIO_setOutputLowOnPin(GPIO_PORT_P4, GPIO_PIN_ALL8);
    GPIO_setOutputLowOnPin(GPIO_PORT_P5, GPIO_PIN_ALL8);
    GPIO_setOutputLowOnPin(GPIO_PORT_P6, GPIO_PIN0 | GPIO_PIN1 | GPIO_PIN2);


    // Configure P4.2 input for CAN interrupt
    GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P4, GPIO_PIN2);
    GPIO_selectInterruptEdge(GPIO_PORT_P4, GPIO_PIN2, GPIO_HIGH_TO_LOW_TRANSITION);
    GPIO_clearInterrupt(GPIO_PORT_P4, GPIO_PIN2);
    GPIO_enableInterrupt(GPIO_PORT_P4, GPIO_PIN2);

    GPIO_setOutputHighOnPin(GPIO_PORT_P4, GPIO_PIN1);       //MCU P4.1 CAN reset pin




    // Disable the GPIO power-on default high-impedance mode
    // to activate previously configured port settings
    PMM_unlockLPM5();
}
/**
 * main.c
 */
int main(void)
{
	WDTCTL = WDTPW | WDTHOLD;	// stop watchdog timer
	
    init_gpio();                                    // Set up GPIOs for SPI and TCAN4550 connections
    init_clock();                                   // Set up the system clocks for 16 MHz (on the MSP430)
    init_spi_peripheral();                                     // Initialize the SPI hardware module for 2 MHz SPI
    GPIO_clearInterrupt(GPIO_PORT_P4, GPIO_PIN2);   // Clear any interrupts on pin 4.2 before we enable global interrupts
    __enable_interrupt();

    init_can();                                     // Run the main MCAN configuration sequence. The bulk of the configuration is in this!

    /* Define the CAN message we want to send*/
    TCAN4x5x_MCAN_TX_Header header = {0};           // Remember to initialize to 0, or you'll get random garbage!
    uint8_t data[4] = {0x55, 0x66, 0x77, 0x88};     // Define the data payload
    header.DLC = MCAN_DLC_4B;                       // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
    header.id = 0x144;                              // Set the ID
    header.FDF = 1;                                 // CAN FD frame enabled
    header.BRS = 1;                                 // Bit rate switch enabled
    header.EFC = 0;
    header.MM  = 0;
    header.RTR = 0;
    header.XTD = 0;                                 // We are not using an extended ID in this example
    header.ESI = 0;                                 // Error state indicator


    TCAN4x5x_MCAN_WriteTXBuffer(0, &header, data);  // This function actually writes the header and data payload to the TCAN's MRAM in the specified TX queue number. It returns the bit necessary to write to TXBAR,
                                                    // but does not necessarily require you to use it. In this example, we won't, so that we can send the data queued up at a later point.

    /* Let's make a different CAN message */
    data[0] = 0x11;
    data[1] = 0x22;
    data[2] = 0x33;
    data[3] = 0x44;                                 // Define the data payload

    header.DLC = MCAN_DLC_4B;                       // Set the DLC to be equal to or less than the data payload (it is ok to pass a 64 byte data array into the WriteTXFIFO function if your DLC is 8 bytes, only the first 8 bytes will be read)
    header.id = 0x123;                              // Set the ID
    header.FDF = 1;                                 // CAN FD frame enabled
    header.BRS = 1;                                 // Bit rate switch enabled
    header.EFC = 0;
    header.MM  = 0;
    header.RTR = 0;
    header.XTD = 0;                                 // We are not using an extended ID in this example
    header.ESI = 0;                                 // Error state indicator

    TCAN4x5x_MCAN_WriteTXBuffer(1, &header, data);  // This line writes the data and header to TX FIFO 1
    TCAN4x5x_MCAN_TransmitBufferContents(1);        // Request that TX Buffer 1 be transmitted


    TCAN4x5x_MCAN_TransmitBufferContents(0);        // Now we can send the TX FIFO element 0 data that we had queued up earlier but didn't send.

    while (1)
    {
        TCAN4x5x_MCAN_TransmitBufferContents(0);        // Now we can send the TX FIFO element 0 data that we had queued up earlier but didn't send.
        __delay_cycles(16000000);
        if (TCAN_Int_Cnt > 0 )
        {
            TCAN_Int_Cnt--;
            TCAN4x5x_Device_Interrupts dev_ir = {0};            // Define a new Device IR object for device (non-CAN) interrupt checking
            TCAN4x5x_MCAN_Interrupts mcan_ir = {0};             // Setup a new MCAN IR object for easy interrupt checking
            TCAN4x5x_Device_ReadInterrupts(&dev_ir);            // Read the device interrupt register
            TCAN4x5x_MCAN_ReadInterrupts(&mcan_ir);             // Read the interrupt register

            if (dev_ir.SPIERR)                                  // If the SPIERR flag is set
                TCAN4x5x_Device_ClearSPIERR();                  // Clear the SPIERR flag

            if (mcan_ir.RF0N)                                   // If a new message in RX FIFO 0
            {
                TCAN4x5x_MCAN_RX_Header MsgHeader = {0};        // Initialize to 0 or you'll get garbage
                uint8_t numBytes = 0;                           // Used since the ReadNextFIFO function will return how many bytes of data were read
                uint8_t dataPayload[64] = {0};                  // Used to store the received data

                TCAN4x5x_MCAN_ClearInterrupts(&mcan_ir);        // Clear any of the interrupt bits that are set.

                numBytes = TCAN4x5x_MCAN_ReadNextFIFO( RXFIFO0, &MsgHeader, dataPayload);   // This will read the next element in the RX FIFO 0

                // numBytes will have the number of bytes it transfered in it. Or you can decode the DLC value in MsgHeader.DLC
                // The data is now in dataPayload[], and message specific information is in the MsgHeader struct.
                if (MsgHeader.id == 0x0AA)      // Example of how you can do an action based off a received address
                {
                    // Do something
                }
            }
        }
    }

}

//******************************************************************************
//
//This is the PORT2_VECTOR interrupt vector service routine
//
//******************************************************************************
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=PORT4_VECTOR
__interrupt
#elif defined(__GNUC__)
__attribute__((interrupt(PORT4_VECTOR)))
#endif
void P4_ISR (void)
{
    TCAN_Int_Cnt++;

    GPIO_clearInterrupt (GPIO_PORT_P4, GPIO_PIN2);
    // Toggle P1.0 output
    GPIO_toggleOutputOnPin (GPIO_PORT_P1, GPIO_PIN0);
    GPIO_setOutputHighOnPin(GPIO_PORT_P3, GPIO_PIN1);

}

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我在 TCAN4x5x_SPI.h 文件中更改了以下内容:

    //定义了用于 MSP430 SPI 端口的 GPIO 端口和引脚。
    #define SPI_CS_GPIO 端口 GPIO 端口 P2
    #define SPI_CS_GPIO 引脚 GPIO 引脚 PIN7
    #define SPI_HW_ADDR EUSCI_B1_BASE

    尽管 SPI_CS (黄色信号)上的活动不是我所期待的。 它未显示活动低电平。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    > EUSCI_B_SPI_select4引脚功能(EUSCI_B1_BASE,0x00);

    这将设置 UCSTEM=0,这会导致 SPI 单元监控 STE 是否存在总线冲突,而不是驱动它[参考 FR2用户指南(SLAU445I)第23.3.3.1节]。 这是一种比较古咒的用法,我很确定  这正是你的习惯。

    将0x00替换为 EUSCI_B_SPI_ENABLE_SIGNAL_4WIRE_SLAVE [它=UCSTEM]。

    ---

    未经请求:我怀疑您根本不想使用4Pin 模式。 从 TCAN4550数据表(SLLSF91A)图35 (例如)中判断,设备预计 NCS 将在整个事务中被断言,而 UCSTEM=1则对每个字节进行断言/断言[参考 FR2 UG 图23-4]。

    我建议您使用3引脚模式,将 STE 引脚(或其他一些引脚)配置为 GPIO,并自行控制 NCS。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    是的,3针模式 清理了 SPI CS,生产固件使用了该模式。 从不考虑查看 LP-MSP430FR6989 SPI 信号以了解如何实施4线 SPI。 接下来我将看一下 CAN 信号。 谢谢你。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我看到 SPI CS 和 SPI CLK 的 TTL 电压级别。 但我看不到 SPI MOSI 的 TTL 级别。 TCAN EVM 没有接收中断。 为什么会这样? 我将此线程标记为“已解决”,但仍需要帮助。 谢谢

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    这看起来像是一场公共汽车冲突,就好像 TCAN4550在驱动 SDI 或其他东西一样。

    如果断开 MOSI 导线,您是否看到相同的波形? 该实验将指向 Launchpad 或 EVM。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我移除了 TCAN EVM 的所有跳线,并且只查看 MSP430 SPI 信号。 只有 SPI_CLK 和 SPI CS 才是 TTL 信号。 移动信号的 TTL 与之前发布的图片不同。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我没有看到你如何从 LP 自身获得这种效果,所以我使用你的 main.c 和来自 TCAN 产品页面的.zip 文件将其组合到了启动板上(我没有 TCAN 设备)。

    我看到一个相当正常的波形。 这是 MOSI 和 SCK (我的范围只有2个通道)。

    我不知道我们在采取什么不同的做法,但这也许表明成功是可能的。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    我的一个示波器探头的衰减翻了10倍。 感谢您的帮助。 我看到了 MOSI 中有意义的级别,谢谢。

  • 请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

    已经到了那里,完成了(:-))。 我很高兴你能让它发挥作用。