嗨,社区,
最近几天,我一直在尝试配置 ADC 来测量电池电量。 所以我在这里使用参考电压发生器作为 ADC 的参考。我们知道,在参考局部缓冲器稳定下来之前,我们无法启动 ADC。 所以我想有两种方法可以做到这一点
1.在 REFCTL 中使用 REFGENRDY 位
2.使用 ADCRDYIFG 中断
由于我在非常电源相关的应用中工作,所以我采用了 ADC 就绪中断。但是,尽管我启用了该中断并以正确的方式设置了大部分内容(我认为) ,但 ADCRDY 中断未被触发。还有一个术语称为样本触发器(这可以帮助 ADCRDYIFG) 但我不知道如何设置信号
2.我也不能用多个 ADCMTL 寄存器和 CSTADDRX 位来总结。这两个寄存器之间的连接是什么。
因此,请您对我的错误和我的问题发表看法。
/* --COPYRIGHT--,BSD_EX
* Copyright (c) 2015, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*******************************************************************************
*
* MSP430 CODE EXAMPLE DISCLAIMER
*
* MSP430 code examples are self-contained low-level programs that typically
* demonstrate a single peripheral function or device feature in a highly
* concise manner. For this the code may rely on the device's power-on default
* register values and settings such as the clock configuration and care must
* be taken when combining code from several examples to avoid potential side
* effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
* for an API functional library-approach to peripheral configuration.
*
* --/COPYRIGHT--*/
//******************************************************************************
// MSP430FR5x9x Demo - ADC12, Sample A1, AVcc Ref, Set P1.0 if A1 > 0.5*AVcc
//
// Description: A single sample is made on A1 with reference to AVcc.
// Software sets ADC12SC to start sample and conversion - ADC12SC
// automatically cleared at EOC. ADC12 internal oscillator times sample (16x)
// and conversion. In Mainloop MSP430 waits in LPM0 to save power until ADC12
// conversion complete, ADC12_ISR will force exit from LPM0 in Mainloop on
// reti. If A1 > 0.5*AVcc, P1.0 set, else reset. The full, correct handling of
// and ADC12 interrupt is shown as well.
//
//
// MSP430FR5994
// -----------------
// /|\| XIN|-
// | | |
// --|RST XOUT|-
// | |
// >---|P1.1/A1 P1.0|-->LED
//
// William Goh
// Texas Instruments Inc.
// October 2015
// Built with IAR Embedded Workbench V6.30 & Code Composer Studio V6.1
//******************************************************************************
#include <msp430.h>
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
// GPIO Setup
P1OUT &= ~BIT0; // Clear LED to start
P1DIR |= BIT0; // Set P1.0/LED to output
P1SEL1 |= BIT2; // Configure P1.1 for ADC
P1SEL0 |= BIT2;
// Disable the GPIO power-on default high-impedance mode to activate
// previously configured port settings
PM5CTL0 &= ~LOCKLPM5;
// Configure Ref voltage generator
REFCTL0 |=REFVSEL_3|REFON;
// Configure ADC12
ADC12CTL0 = ADC12SHT0_2 | ADC12ON; // Sampling time, S&H=16, ADC12 on
ADC12CTL1 = ADC12SHP; // Use sampling timer
ADC12CTL2 |= ADC12RES_2; // 12-bit conversion results
ADC12MCTL1|= ADC12INCH_2|ADC12VRSEL_1; // A1 ADC input select; Vref=AVCC
ADC12IER0 |= ADC12IE0; // Enable ADC conv complete interrupt
ADC12IER2 |=ADC12RDYIE;
__enable_interrupt();
while (1)
{
while(!(REFCTL0 & REFGENRDY)); // Wait for reference generator
__delay_cycles(5000);
ADC12CTL0 |= ADC12ENC
| ADC12SC; // Start sampling/conversion
__bis_SR_register(LPM0_bits | GIE); // LPM0, ADC12_ISR will force exit
__no_operation(); // For debugger
}
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = ADC12_B_VECTOR
__interrupt void ADC12_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_B_VECTOR))) ADC12_ISR (void)
#else
#error Compiler not supported!
#endif
{
switch(__even_in_range(ADC12IV, ADC12IV__ADC12RDYIFG))
{
case ADC12IV__NONE: __no_operation(); break; // Vector 0: No interrupt
case ADC12IV__ADC12OVIFG: __no_operation(); break; // Vector 2: ADC12MEMx Overflow
case ADC12IV__ADC12TOVIFG: __no_operation(); break; // Vector 4: Conversion time overflow
case ADC12IV__ADC12HIIFG: __no_operation(); break; // Vector 6: ADC12BHI
case ADC12IV__ADC12LOIFG: __no_operation(); break; // Vector 8: ADC12BLO
case ADC12IV__ADC12INIFG: __no_operation(); break; // Vector 10: ADC12BIN
case ADC12IV__ADC12IFG0: // Vector 12: ADC12MEM0 Interrupt
if (ADC12MEM0 >= 0x7ff) // ADC12MEM0 = A1 > 0.5AVcc?
P1OUT |= BIT0; // P1.0 = 1
else
P1OUT &= ~BIT0; // P1.0 = 0
// Exit from LPM0 and continue executing main
__bic_SR_register_on_exit(LPM0_bits);
__no_operation(); break;
case ADC12IV__ADC12IFG1: __no_operation(); break; // Vector 14: ADC12MEM1
case ADC12IV__ADC12IFG2: __no_operation(); break; // Vector 16: ADC12MEM2
case ADC12IV__ADC12IFG3: __no_operation(); break; // Vector 18: ADC12MEM3
case ADC12IV__ADC12IFG4: __no_operation(); break; // Vector 20: ADC12MEM4
case ADC12IV__ADC12IFG5: __no_operation(); break; // Vector 22: ADC12MEM5
case ADC12IV__ADC12IFG6: __no_operation(); break; // Vector 24: ADC12MEM6
case ADC12IV__ADC12IFG7: __no_operation(); break; // Vector 26: ADC12MEM7
case ADC12IV__ADC12IFG8: __no_operation(); break; // Vector 28: ADC12MEM8
case ADC12IV__ADC12IFG9: __no_operation(); break; // Vector 30: ADC12MEM9
case ADC12IV__ADC12IFG10: __no_operation(); break; // Vector 32: ADC12MEM10
case ADC12IV__ADC12IFG11: __no_operation(); break; // Vector 34: ADC12MEM11
case ADC12IV__ADC12IFG12: __no_operation(); break; // Vector 36: ADC12MEM12
case ADC12IV__ADC12IFG13: __no_operation(); break; // Vector 38: ADC12MEM13
case ADC12IV__ADC12IFG14: __no_operation(); break; // Vector 40: ADC12MEM14
case ADC12IV__ADC12IFG15: __no_operation(); break; // Vector 42: ADC12MEM15
case ADC12IV__ADC12IFG16: __no_operation(); break; // Vector 44: ADC12MEM16
case ADC12IV__ADC12IFG17: __no_operation(); break; // Vector 46: ADC12MEM17
case ADC12IV__ADC12IFG18: __no_operation(); break; // Vector 48: ADC12MEM18
case ADC12IV__ADC12IFG19: __no_operation(); break; // Vector 50: ADC12MEM19
case ADC12IV__ADC12IFG20: __no_operation(); break; // Vector 52: ADC12MEM20
case ADC12IV__ADC12IFG21: __no_operation(); break; // Vector 54: ADC12MEM21
case ADC12IV__ADC12IFG22: __no_operation(); break; // Vector 56: ADC12MEM22
case ADC12IV__ADC12IFG23: __no_operation(); break; // Vector 58: ADC12MEM23
case ADC12IV__ADC12IFG24: __no_operation(); break; // Vector 60: ADC12MEM24
case ADC12IV__ADC12IFG25: __no_operation(); break; // Vector 62: ADC12MEM25
case ADC12IV__ADC12IFG26: __no_operation(); break; // Vector 64: ADC12MEM26
case ADC12IV__ADC12IFG27: __no_operation(); break; // Vector 66: ADC12MEM27
case ADC12IV__ADC12IFG28: __no_operation(); break; // Vector 68: ADC12MEM28
case ADC12IV__ADC12IFG29: __no_operation(); break; // Vector 70: ADC12MEM29
case ADC12IV__ADC12IFG30: __no_operation(); break; // Vector 72: ADC12MEM30
case ADC12IV__ADC12IFG31: __no_operation(); break; // Vector 74: ADC12MEM31
case ADC12IV__ADC12RDYIFG:
ADC12CTL0 |= ADC12ENC | ADC12SC; // Start sampling/conversion
__no_operation();
break; // Vector 76: ADC12RDY
default: __no_operation(); break;
}
}