请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:MSP432P401R 主题中讨论的其他部件:CC3100,
您好,
我想通过外部电源连接MSP432。
我应该使用连接到J7的5V直流电池还是连接到J6的3.3V电池?
在MSP432上连接外部电源而不是USB笔记本电脑电源时,是否需要进行任何其他更改?
我的msp432也连接到CC3100 WiFi扩展 器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我想通过外部电源连接MSP432。
我应该使用连接到J7的5V直流电池还是连接到J6的3.3V电池?
在MSP432上连接外部电源而不是USB笔记本电脑电源时,是否需要进行任何其他更改?
我的msp432也连接到CC3100 WiFi扩展 器。