请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:MSP430FR2633 您好,champs:
对于作为Captivate控制器的最低配置(BOM),是否需要外部32.768kHz晶体XT1?
什么是应用程序,需要XT1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,champs:
对于作为Captivate控制器的最低配置(BOM),是否需要外部32.768kHz晶体XT1?
什么是应用程序,需要XT1?