请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:MSP430F5659 您好,
内部REFOCLK与典型的外部50 ppm晶体振荡器相比,在以下方面如何:(i)准确度,(ii)电流消耗,(iii)稳健性?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
内部REFOCLK与典型的外部50 ppm晶体振荡器相比,在以下方面如何:(i)准确度,(ii)电流消耗,(iii)稳健性?
[报价用户="Boaz Aizenshtark">部件号: MSP430F5659
您好,
内部REFOCLK在以下方面与典型的外部50 ppm晶体振荡器相比如何:(i)精度,(ii)电流消耗,(iii)稳健性?[/QUOT]
一般来说,MSP430内部时钟源与外部XT1/XT2相关的功耗和精度较低。 如果您对准确性有问题,请直接使用XT2或拆分使用XT2。