请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:MSP430FR2311 MSP430FR231x是否在器件描述符TLV结构中存储了30C/85C温度校准值?
我看到1.5 6.13 部分列出的"ADC 1.5 -V参考电压,温度30°C / ADC"和"ADC-V参考电压和温度85°C",但不清楚这些是使用1.5V参考电压的温度传感器读数,还是仅仅是这些温度下的1.5V参考电压读数。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MSP430FR231x是否在器件描述符TLV结构中存储了30C/85C温度校准值?
我看到1.5 6.13 部分列出的"ADC 1.5 -V参考电压,温度30°C / ADC"和"ADC-V参考电压和温度85°C",但不清楚这些是使用1.5V参考电压的温度传感器读数,还是仅仅是这些温度下的1.5V参考电压读数。