请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他部件:MSP430FR2633, MSP430FR4133, MSP-EXP430FR4133支持路径:/Product/Help with Device Selection/
我需要一个与ATMEGA 16A功能相同的TI微处理器。
我需要参考2017 TI设计竞赛。
因此,如果我有一个与ATMEGA 16A对应的微处理器,我将会非常有必要
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
支持路径:/Product/Help with Device Selection/
我需要一个与ATMEGA 16A功能相同的TI微处理器。
我需要参考2017 TI设计竞赛。
因此,如果我有一个与ATMEGA 16A对应的微处理器,我将会非常有必要