请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:eZ430-T2012 主题中讨论的其他部件: eZ430-F2013
我需要此主板的连接器部件号...我将eZ430用作编程器工具,需要与 eZ430-T2012部件上的相同匹配连接器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我需要此主板的连接器部件号...我将eZ430用作编程器工具,需要与 eZ430-T2012部件上的相同匹配连接器
它是标准1.27 mm (0.05 ")管座,带机加工引脚。 无论如何,eZ430-F2013用户指南显示:
9个常见问题
6. MSP-EZ430U仿真器和MSP-EZ430D目标板之间的连接器的部件号是什么?
管座:MILE-Max 850-10-004-20-0.1万 (Digi-Key部件号ED8650-ND)
插座:铣刀-最大851-93-004-20-0.1万 (Digi-Key部件号ED8850-ND)