Other Parts Discussed in Thread: MSP430FR2033
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
部件号:MSP430FR2033 您好,
我想将 8 MAX3.1856万热电偶温度补偿IC与MSP430fr2033控制器连接起来。 我使用 SPI通信在MAX3.1856万和MSP430fr2033之间进行通信。因此,任何人都可以告诉我基本的想法或流程图。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP430FR2033
您好,
我想将 8 MAX3.1856万热电偶温度补偿IC与MSP430fr2033控制器连接起来。 我使用 SPI通信在MAX3.1856万和MSP430fr2033之间进行通信。因此,任何人都可以告诉我基本的想法或流程图。